We took over the project from K60 to K66. With the same initialization, the interrrupt no longer works. What is the difference.
已解决! 转到解答。
Hi,
I checked the CAN0 and CAN1 interrupt setting code with problem.
As ARM Cortex M4 core shows the interrupt set-enable registers shows the IRQ number (IRQ) with related register:
For the CAN0 interrupt IRQ value from 75 to 80, which need to use NVIC_ISER2 register to enable CAN0 interrupt.
The CAN1 interrupt IRQ value from 94 to 99, which need to use NVIC_ISER2 and NVIC_ISER3 to enable related CAN1 interrupt.
Please refer below code, which is for K70_120MHz product to enable interrupt function:
/***********************************************************************/
/*
* Initialize the NVIC to enable the specified IRQ.
*
* NOTE: The function only initializes the NVIC to enable a single IRQ.
* Interrupts will also need to be enabled in the ARM core. This can be
* done using the EnableInterrupts macro.
*
* Parameters:
* irq irq number to be enabled (the irq number NOT the vector number)
*/
void enable_irq (int irq)
{
int div;
/* Make sure that the IRQ is an allowable number. Right now up to 105 is
* used.
*/
if (irq > 105)
printf("\nERR! Invalid IRQ value passed to enable irq function!\n");
/* Determine which of the NVICISERs corresponds to the irq */
div = irq/32;
switch (div)
{
case 0x0:
NVICICPR0 |= 1 << (irq%32);
NVICISER0 |= 1 << (irq%32);
break;
case 0x1:
NVICICPR1 |= 1 << (irq%32);
NVICISER1 |= 1 << (irq%32);
break;
case 0x2:
NVICICPR2 |= 1 << (irq%32);
NVICISER2 |= 1 << (irq%32);
break;
case 0x3:
NVICICPR3 |= 1 << (irq%32);
NVICISER3 |= 1 << (irq%32);
break;
}
}
Wish it helps.
Best regards,
Ma Hui
Hi,
If you are using K60_120MHz product and port to K66 product, the interrupt vector assignment has changed:
K60_120MHz product CAN0 interrupt vector from 45 to 50, CAN1 interrupt vector from 53 to 58;
K66 product CAN0 interrupt vector from 91 to 96, CAN1 interrupt vector from 110 to 115;
More detailed info, please check each reference manual chapter3.
Wish it helps.
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
thanks for the answers.
I set the numbers correctly. But doesn't work. In the Register i can see the data.
Here my init Code:
MK66F18.h
[...]
CAN0_ORed_Message_buffer_IRQn = 75, /**< CAN0 OR'd message buffers interrupt */
CAN0_Bus_Off_IRQn = 76, /**< CAN0 bus off interrupt */
CAN0_Error_IRQn = 77, /**< CAN0 error interrupt */
CAN0_Tx_Warning_IRQn = 78, /**< CAN0 Tx warning interrupt */
CAN0_Rx_Warning_IRQn = 79, /**< CAN0 Rx warning interrupt */
CAN0_Wake_Up_IRQn = 80, /**< CAN0 wake up interrupt */
[..]
CAN1_ORed_Message_buffer_IRQn = 94, /**< CAN1 OR'd message buffers interrupt */
CAN1_Bus_Off_IRQn = 95, /**< CAN1 bus off interrupt */
CAN1_Error_IRQn = 96, /**< CAN1 error interrupt */
CAN1_Tx_Warning_IRQn = 97, /**< CAN1 Tx warning interrupt */
CAN1_Rx_Warning_IRQn = 98, /**< CAN1 Rx warning interrupt */
CAN1_Wake_Up_IRQn = 99 /**< CAN1 wake up interrupt */
[...]
I init the Can 1 and 2:
CANX->CTRL1 &= ~(CAN_CTRL1_CLKSRC_MASK); CTRL1[CLK_SRC] bit. (OSCCLK)
CANX->MCR &= ~(CAN_MCR_MDIS_MASK);
while((CAN_MCR_LPMACK_MASK & CANX->MCR));
while(!(CAN_MCR_FRZACK_MASK & CANX->MCR));
CANX->MCR |= CAN_MCR_IRMQ_MASK;
CANX->MCR |= CAN_MCR_WRNEN_MASK;
CANX->MCR &= ~(CAN_MCR_SRXDIS_MASK);
CANX->MCR |= CAN_MCR_AEN_MASK;
CANX->MCR |= CAN_MCR_LPRIOEN_MASK;
can_init_BAUD( baudrateKHz , X , 12000000 );
I init the CAN 0 Int.:
NVIC->ICPR[ 0 ] = ( NVIC->ICPR[ 0 ] & ~(((uint32_t)0x07)<<29)) | (((uint32_t)0x07)<<29); /* Clear pending interrupt CAN0 */
NVIC->ISER[ 0 ] = ( NVIC->ISER[ 0 ] & ~(((uint32_t)0x07)<<29)) | (((uint32_t)0x07)<<29); /* enable interrupt CAN0 */
NVIC->ICPR[ 1 ] = ( NVIC->ICPR[ 1 ] & ~(((uint32_t)0x1F)<<0)) | ((uint32_t)0x1F); /* Clear pending interrupt CAN0 */
NVIC->ISER[ 1 ] = ( NVIC->ISER[ 1 ] & ~(((uint32_t)0x1F)<<0)) | ((uint32_t)0x1F); /* enable interrupt CAN0 */
I init the CAN 1 Int.:
NVIC->ICPR[ 1 ] = ( NVIC->ICPR[ 1 ] & ~(((uint32_t)0xFF)<<5)) | (((uint32_t)0xFF)<<5); /* Clear pending interrupt CAN1*/
NVIC->ISER[ 1 ] = ( NVIC->ISER[ 1 ] & ~(((uint32_t)0xFF)<<5)) | (((uint32_t)0xFF)<<5); /* enable interrupt CAN1*/
Hi,
I checked the CAN0 and CAN1 interrupt setting code with problem.
As ARM Cortex M4 core shows the interrupt set-enable registers shows the IRQ number (IRQ) with related register:
For the CAN0 interrupt IRQ value from 75 to 80, which need to use NVIC_ISER2 register to enable CAN0 interrupt.
The CAN1 interrupt IRQ value from 94 to 99, which need to use NVIC_ISER2 and NVIC_ISER3 to enable related CAN1 interrupt.
Please refer below code, which is for K70_120MHz product to enable interrupt function:
/***********************************************************************/
/*
* Initialize the NVIC to enable the specified IRQ.
*
* NOTE: The function only initializes the NVIC to enable a single IRQ.
* Interrupts will also need to be enabled in the ARM core. This can be
* done using the EnableInterrupts macro.
*
* Parameters:
* irq irq number to be enabled (the irq number NOT the vector number)
*/
void enable_irq (int irq)
{
int div;
/* Make sure that the IRQ is an allowable number. Right now up to 105 is
* used.
*/
if (irq > 105)
printf("\nERR! Invalid IRQ value passed to enable irq function!\n");
/* Determine which of the NVICISERs corresponds to the irq */
div = irq/32;
switch (div)
{
case 0x0:
NVICICPR0 |= 1 << (irq%32);
NVICISER0 |= 1 << (irq%32);
break;
case 0x1:
NVICICPR1 |= 1 << (irq%32);
NVICISER1 |= 1 << (irq%32);
break;
case 0x2:
NVICICPR2 |= 1 << (irq%32);
NVICISER2 |= 1 << (irq%32);
break;
case 0x3:
NVICICPR3 |= 1 << (irq%32);
NVICISER3 |= 1 << (irq%32);
break;
}
}
Wish it helps.
Best regards,
Ma Hui