Hello,
I am trying to implement a pulse counter by using LPTMR0 of MK64FN1M0VLL12 chip. I want to use PTC5 pin for pulse counting. Here is my code:
//enable clock for PORTC
SIM->SCGC5 |= (1UL << 11);
//set PORTC pin 5 as pulse counter pin (PIN ALT3: LPTMR0_ALT2)
PORTC->PCR[5] = (1UL << 9) | (1UL << 8);
//enable clock for LPTMR0
SIM->SCGC5 |= (1UL << 0);
// reset LPTMR
LPTMR0->CSR = 0;
LPTMR0->PSR = 0;
LPTMR0->CMR = 0; // no need for compare value because i will use counter in free running mode
//select LPTMR0_ALT2 (PTC5) as pulse counter pin
LPTMR0->CSR |= (1 << 5);
//counter is free running
LPTMR0->CSR |= (1 << 2);
//select pulse counter mode
LPTMR0->CSR |= (1 << 1);
//pulse counter input pin directly clocks counter value (bypass glitch filter)
LPTMR0->PSR = (1 << 2);
//enable LPTMR module
LPTMR0->CSR |= (1 << 0);
while (true) {
LPTMR0->CNR = 1; // write any value first to CNR to read CNR value
printf("counter value: %lu\r\n", LPTMR0->CNR);
wait(1.0f);
}
I am expecting this code to return the current pulse count on pulse pin every second. But if I connect PTC5 to GND (no pulse) the pulse counter starts to increment (16000 after 1 second). My question is why it does behave like this? It should not detect any pulses because it is connected to GND. Also when I connect the pin to +3.3V it does behave like this. Am I missing some point here?
已解决! 转到解答。
Thanks for your support! Your project compiled and worked well for me too. The problem I had was this line
wait(1.0f);
The version of mbed library internally manipulates LPTMR0 when using the wait(); function. That was the reason why I was experiencing strange behaviour. With the latest version of mbed it works very well.
Hi Armin Bego,
I use your code and test it on my TWR-K64, when I connect PTC5 to ground, the out put data is always 0, and never increase, but when I connect PTC5 to a PWM wave, the CNR can be increased. It works ok on my side, I think you should check your ground, whether it has the little pulse?
Beside, I attached my test project, you can use my project(KDS3.0) and run it on your side.
If you still have question, please contact me!
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for your effort Jingjing Zhou,
i checked my ground and +3.3V signal. There is no noise. Also I have tried my code on another FRDM-K64 board, it behaves the same. I also tried to compile it with online mbed compiler, no succes.
Hi Armin Bego,
I also test it on our FRDM-K64, it also woks ok, attached is the project for K64, it will printf the result, following is my FRDM-K64 test result:
....
counter value: 1903
counter value: 1951
counter value: 1995
counter value: 2041
counter value: 2086
counter value: 2130
counter value: 2175
counter value: 2220
counter value: 2265
counter value: 2310
counter value: 2355
counter value: 2400
counter value: 2445
counter value: 2494
counter value: 2539
counter value: 2583
counter value: 2623
counter value: 2625
counter value: 2625
counter value: 2625
counter value: 2625
counter value: 2625
counter value: 2625
counter value: 2625
counter value: 2625
counter value: 2625
counter value: 2625
counter value: 2625
counter value: 2625
counter value: 2625
counter value: 2625
counter value: 2625
counter value: 2625
counter value: 2625
counter value: 2625
When I connect it to the PWM, it will increase, if I connect it to the ground, the vaulue will not increase, and stopped in 2625, you can use my project and test it on your FRDM-K64.
Besides, take care, PTC5 is the pin15 in J1, you should make sure you connect the correct pin.
Wish it helps you!
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for your support! Your project compiled and worked well for me too. The problem I had was this line
wait(1.0f);
The version of mbed library internally manipulates LPTMR0 when using the wait(); function. That was the reason why I was experiencing strange behaviour. With the latest version of mbed it works very well.