Hi All,
Now I am trying to use the SPI communication on TWR-K60N512 board to control the a DOGS-102-6 LCD.
I edited the SPI sample code under /mqx/example/spi, and connected elevator board signal to the LCD through:
(SPI2)
Elevator board LCD
Pin 7 on J6 CLK
Pin 9 on J6 CS
Pin 10 on J6 MOSI
Now the problem is that there is not clock signal and data signal from Pin7 and Pin9.
The code is as following:
spifd = fopen ("spi2:" NULL);
if (NULL == spifd)
{
printf ("Error opening SPI driver!\n");
_time_delay (200L);
_task_block ();
}
/* Display baud rate */
printf ("Current baud rate ... ");
if (SPI_OK == ioctl (spifd, IO_IOCTL_SPI_GET_BAUD, ¶m))
{
printf ("%d Hz\n", param);
} else {
printf ("ERROR\n");
}
/* Set a different rate */
param = 500000;
printf ("Changing the baud rate to %d Hz ... ", param);
if (SPI_OK == ioctl (spifd, IO_IOCTL_SPI_SET_BAUD, ¶m))
{
printf ("OK\n");
} else {
printf ("ERROR\n");
}
/* Display baud rate */
printf ("Current baud rate ... ");
if (SPI_OK == ioctl (spifd, IO_IOCTL_SPI_GET_BAUD, ¶m))
{
printf ("%d Hz\n", param);
} else {
printf ("ERROR\n");
}
/* Set clock mode */
param = SPI_CLK_POL_PHA_MODE0;
printf ("Setting clock mode to %s ... ", clock_mode[param]);
if (SPI_OK == ioctl (spifd, IO_IOCTL_SPI_SET_MODE, ¶m))
{
printf ("OK\n");
} else {
printf ("ERROR\n");
}
/* Get clock mode */
printf ("Getting clock mode ... ");
if (SPI_OK == ioctl (spifd, IO_IOCTL_SPI_GET_MODE, ¶m))
{
printf ("%s\n", clock_mode[param]);
} else {
printf ("ERROR\n");
}
/* Set big endian */
param = SPI_DEVICE_BIG_ENDIAN;
printf ("Setting endian to %s ... ", param == SPI_DEVICE_BIG_ENDIAN ? "SPI_DEVICE_BIG_ENDIAN" : "SPI_DEVICE_LITTLE_ENDIAN");
if (SPI_OK == ioctl (spifd, IO_IOCTL_SPI_SET_ENDIAN, ¶m))
{
printf ("OK\n");
} else {
printf ("ERROR\n");
}
/* Get endian */
printf ("Getting endian ... ");
if (SPI_OK == ioctl (spifd, IO_IOCTL_SPI_GET_ENDIAN, ¶m))
{
printf ("%s\n", param == SPI_DEVICE_BIG_ENDIAN ? "SPI_DEVICE_BIG_ENDIAN" : "SPI_DEVICE_LITTLE_ENDIAN");
} else {
printf ("ERROR\n");
}
/* Set transfer mode */
param = SPI_DEVICE_MASTER_MODE;
printf ("Setting transfer mode to %s ... ", device_mode[param]);
if (SPI_OK == ioctl (spifd, IO_IOCTL_SPI_SET_TRANSFER_MODE, ¶m))
{
printf ("OK\n");
} else {
printf ("ERROR\n");
}
/* Get transfer mode */
printf ("Getting transfer mode ... ");
if (SPI_OK == ioctl (spifd, IO_IOCTL_SPI_GET_TRANSFER_MODE, ¶m))
{
printf ("%s\n", device_mode[param]);
} else {
printf ("ERROR\n");
}
/* Clear statistics */
printf ("Clearing statistics ... ");
if (SPI_OK == ioctl (spifd, IO_IOCTL_SPI_CLEAR_STATS, NULL))
{
printf ("OK\n");
} else {
printf ("ERROR\n");
}
/* Get statistics */
printf ("Getting statistics:\n");
if (SPI_OK == ioctl (spifd, IO_IOCTL_SPI_GET_STATS, &stats))
{
printf ("Interrupts: %d\n", stats.INTERRUPTS);
printf ("Rx packets: %d\n", stats.RX_PACKETS);
printf ("Rx overflow: %d\n", stats.RX_OVERFLOWS);
printf ("Tx packets: %d\n", stats.TX_PACKETS);
printf ("Tx aborts : %d\n", stats.TX_ABORTS);
printf ("Tx underflow: %d\n", stats.TX_UNDERFLOWS);
} else {
printf ("ERROR\n");
}
/* Write a byte*/
send_buffer[0] = 0x40;
/* Write instruction */
do{
result = fwrite (send_buffer, 1, 1, spifd);
}while( result < 1);
fflush (spifd);
Thank you.
已解决! 转到解答。