K22: LPTMR TCF overhead of 2 ms with LPO?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K22: LPTMR TCF overhead of 2 ms with LPO?

900 次查看
troelsoesteraa
Contributor III

Hi,

Device is MK22FN256VLL12, the LPTMR is currently using the LPO (1 kHz) with prescaler bypassed, running in time counter mode. What I am experiencing is about 2 ms overhead regardless of CMR value, e.g. until TCF is set. I check the LPO on PTE0 using the following setup:
SIM->SOPT1 |= SIM_SOPT1_OSC32KSEL(3) | SIM_SOPT1_OSC32KOUT(1);
The waveform looks as follows:
SCR05.PNG
So about 1% slower, which is well within acceptable.

In the following, the clock output on PTE0 is disabled, it just works as a normal GPIO, configured as output
My LPTMR setups is as follows:

void LPTMR_init(void)

{

   SIM->SCGC5 |= SIM_SCGC5_LPTMR_MASK;

   LPTMR0->CSR = 0;

   LPTMR0->PSR = LPTMR_PSR_PCS(1) | LPTMR_PSR_PBYP_MASK;

}

The LPTMR delay function looks like this:

void LPTMR_delay(uint16_t uValue)

{

   LPTMR0->CMR = LPTMR_CMR_COMPARE(uValue);

   LPTMR0->CSR |= LPTMR_CSR_TEN_MASK;

   while(!(LPTMR0->CSR & LPTMR_CSR_TCF_MASK));
   LPTMR0->CSR &= ~LPTMR_CSR_TEN_MASK;

   GPIOE->PTOR = GPIO_PIN(0);

}

The function calling the LPTMR_delay is as follows:
do

{

   LPTMR_delay(10);

}

while(1);

This is just called from main. The ONLY other ISR running at 20 ms intervals is the SysTick ISR, which just increases a counter and nothing else. The results when monitoring PTE0 using a scope, is as follows:
SCR07.PNG

So what ought to be 10 ms toggle intervals is now approximately 12 ms intervals.

Any suggestions why I have an overhead of 2 ms and what I've misunderstood about the LPTMR?

Thanks a lot.

标记 (5)
0 项奖励
回复
2 回复数

780 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

According to my understanding: When 1kHz LPO is used, LPTMR0->CMR=0x09 will lead 10ms timeout.

40.4.4 LPTMR compare.png

Additionally: When the LPTMR is enabled, the first increment will take an additional one or two prescaler clock cycles due to synchronization logic.

40.4.3.2 Prescaler bypassed.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

780 次查看
troelsoesteraa
Contributor III

In addition to this I tested with the 4 MHz fast IRC as clock for the LPTMR, downscaled to 1 MHz by the MCG, doing the following:

// Disable fast IRC (4 MHz) when FRDRIV is changed
MCG->C2 &= ~MCG_C2_IRCS_MASK;
    
// Divide by 4 to bring clock speed to 1 MHz.
// Make sure to clear any previous setting (reset default is 2!).
MCG->SC &= ~MCG_SC_FCRDIV_MASK;
MCG->SC |= MCG_SC_FCRDIV(2);

// Enable fast IRC again.
MCG->C2 |= MCG_C2_IRCS_MASK;
    
// Enable active IRC as MCGIRCLK for use with LPTMR.
MCG->C1 |= MCG_C1_IRCLKEN_MASK;

Then I configured PSR as follows:
LPTMR0->PSR = LPTMR_PSR_PCS(0) | LPTMR_PSR_PBYP_MASK;

Otherwise, the code is unchanged. The overhead with this configuration is about 2 us, not 2 ms, so quite acceptable!

0 项奖励
回复