JTAG pins on KL34 family?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG pins on KL34 family?

725件の閲覧回数
paulkafig
Contributor II

OK, this is going to seem like a dumb question, but where are the JTAG pins on this part? For example, MKL34Z64VLL4.  I looked through the data sheet and don't see anything about JTAG. I know I have to be missing it. Data sheet attached.

Thanks,

Paul

タグ(2)
0 件の賞賛
返信
3 返答(返信)

607件の閲覧回数
mjbcswitzerland
Specialist V

Paul

The KL parts have SWD (single wire debug) and not JTAG (they also do not have EzPort).

JTAG is available (as well as SWD) in the Cortex M4 parts (like K60). Some of the larger K parts also have trace pins too.

Regards

Mark

607件の閲覧回数
paulkafig
Contributor II

Thank you, Mark. That makes sense now; thought I was losing my mind (although the two are not mutually exclusive)...

Is this the cable used for SWD? Someone recommended it and I want to make sure I'm getting the right thing.

TC2030-CTX 6-Pin Cable for ARM Cortex - Tag Connect 

Best regards,
Paul

0 件の賞賛
返信

607件の閲覧回数
mjbcswitzerland
Specialist V

Paul

I don't know which cable is most suited for you - it probably depends on what is available on your KL34 HW.
The FRDM boards tend to have a 0.05" pitch 10 pin connector which can be directly connected to by various debuggers which looks something like this:

pastedImage_1.png

Whether something special is needed between this and the debugger will depend on whether they already match or not.

Regards

Mark

0 件の賞賛
返信