Is the TRNG on the K64, K65, K65 NIST compliant?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is the TRNG on the K64, K65, K65 NIST compliant?

490件の閲覧回数
RussellPead
Contributor II

Is the TRNG on the next generation Kinetis K6x devices NIST compliant? This is for a medical company so security is critically important.

ラベル(1)
0 件の賞賛
1 返信

334件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I think K64/K65/K66 RNGA module is compliant with NIST.

There with below description from RNGA module chapter of related reference manual:

It is important to note there is no known cryptographic proof showing this is a secure method of generating random data. In fact, there may be an attack against this random number generator if its output is used directly in a cryptographic application. The attack is based on the linearity of the internal shift registers. Therefore, it is highly recommended that this random data produced by this module be used as an entropy source to provide an input seed to a NIST-approved pseudo-random-number generator based on DES or SHA-1 and defined in NIST FIPS PUB 186-2 Appendix 3 and NIST FIPS PUB SP 800-90.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛