Is it possible to use TWR-WIFI-GS1500M base on TWRK70F120M?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to use TWR-WIFI-GS1500M base on TWRK70F120M?

404件の閲覧回数
angli
Contributor I

On the official webpage of the TWR-WIFI-GS1500M said the supported devices are K6x Ethernet Crypto MCUs:

  • K60_100: Kinetis K60 Ethernet 100 MHz MCUs
  • K60_120: Kinetis K60 Ethernet 120/150 MHz MCUs

But TWRK70F120M is similar with K6x MCUs, is it possible to use TWR-WIFI-GS1500M base on TWRK70F120M?

0 件の賞賛
返信
1 返信

298件の閲覧回数
RadekS
NXP Employee
NXP Employee

Freescale TWR-WIFI-GS1500M web pages say that “This peripheral module is designed to be combined and used with other MCU and peripheral modules in the Tower System, including the TWR-K60D100M.”

Nothing blocks you in use different MCU tower board with TWR-WIFI-GS1500M.

You can use TWR-K70F120M board, but you have to check pin configuration – as for any of other MCU boards.

Note: TWR-WIFI-GS1500M board is no longer in production and not recommended for future designs.

I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信