In the PF3000 GUI my board is not showing when i am scanning for devices in the GUI.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In the PF3000 GUI my board is not showing when i am scanning for devices in the GUI.

621 Views
rishav1006115
Contributor I

The LED is blinking on the KITPF3000FRDMEVM board. But when I am scanning in the GUI it is not showing.

0 Kudos
2 Replies

557 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Rishav Kumar,

Would you please tell me which LED is blinking?
If you means the LED on FRDM-KL25Z, then please refer the: LED Status Indicator

LED Status Indicator.png

If you are using Windows8/10, then please refer: Bricking and Recovering OpenSDA Boards in Windows 8 and 10

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

558 Views
rishav1006115
Contributor I

Hello Robin. Actually i have one KITPF3000FRDMEVM. In that when i am using the SDA port it's working perfectly but when i am using KL25Z USB port it's not working. That port is for connecting the PF3000GUI in the computer with the board but it is not scanning my device.  

0 Kudos