I need help to develop the circuit for MKW01Z128 MCU, i have referred the schematic from the data sheet of MKW01Z128 and I'm struck at while developing the circuit for PA_BOOST(Pin 41) in MCU. The application circuit which they given in the data sheet(Pa

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I need help to develop the circuit for MKW01Z128 MCU, i have referred the schematic from the data sheet of MKW01Z128 and I'm struck at while developing the circuit for PA_BOOST(Pin 41) in MCU. The application circuit which they given in the data sheet(Pa

570件の閲覧回数
akshatnegi
Contributor II

I need help to develop the circuit for MKW01Z128 MCU, i have referred the schematic from the data sheet of MKW01Z128 and I'm struck at while developing the circuit for PA_BOOST(Pin 41) in MCU.

The application circuit which they given in the data sheet(Page No:27) was not clear.So i need your help to built that schematic,because PA_BOOST is very much essential for our system to transmit the data through long distance.

ラベル(1)
0 件の賞賛
1 返信

405件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

NXP does not have any specific circuit for the PA, the schematics only show a generic opam but you need to check the requirement that you need in your application in order to select the PA circuit.

Regards

Vicente Gomez

0 件の賞賛