HI
I was using the KE15 development board, and then when I looked at the KE15 SDK driver example, I realized that flexnvm eeprom example could only be configured with 32 byte eeprom, but I wanted to configure 2k eeprom, so I read the reference manual to modify:
1. Modified #define EEPROM_DATA_SET_SIZE_CODE (0x39U) to (0x33U) and redefined #define FLEXNVM_PARTITION_CODE (0x3U).
2. Change the length of the write array and redefine it as #define BUFFER_LEN 16
3. Before: result = FLEXNVM_SetFlexramFunction (& s_flashDriver, kFTFx_FlexramFuncOptAvailableForEeprom);To assign a value : s_flashDriver. FtfxConfig. EepromTotalSize = 0 x800;
Finally, compile and debug, but HardFault_Handler appears
Thank you very much.
Eagan
解決済! 解決策の投稿を見る。
Hi ,could you point out my mistake,and Instruct me how to modify ,thanks ,have great day.
I've found the problem. I've solved it
Thanks
At that time the download program just overwrite, did not forget to erase all, so if you change the parameters of the partition function, to erase all before downloading
Hi Eagan Yu,
Thanks for your updated information.
If you have any questions in the future, welcome to create the new question post, and let us know.
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------