How to set TSEG1 and TSEG2 in register CANBTR1 of KEAZ128?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to set TSEG1 and TSEG2 in register CANBTR1 of KEAZ128?

611件の閲覧回数
w_lingjun
Contributor III
Hi, I'm studying on the MSCAN initialization based on KEAZ128. When I set the register MSCAN_CANBTR1, there are three parts should be set. I don't know how to set the TSEG1 and TSEG2, the reference manual only list the value they can set, but not introduce how to set these two values. For example, the TSEG2 can be set from 001b to 111b, it is only a range, which value should I set? Waiting for your reply. Thank you very much! Best regards, Sarah
0 件の賞賛
1 返信

607件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi w_lingjun

  You are from China, so you can refer to this document, it will help you understand the TSEG1 TSET2 configuration:

https://www.nxpic.org.cn/module/forum/thread-599175-1-1.html

 

 

Wish it helps you!

Best Regards.

Kerry

0 件の賞賛