Our circuit has an issue and for the time being, I want to disable XTAL32 output of K64 and RTC_CLKOUT pin output on PTE26.
Is their any way I can accomplish this without disabling RTC module in the BSP ?
I have tried setting SIM_SOPT2[RTCCLKOUTSEL] = 1 and RTC_CR[CLK0] = 0 which means 32.7KHz will be selected as an output on RTC_CLKOUT pin but then I disable any output on RTC_CLKOUT by doing RTC_CR[CLK0] = 0
mjbcswitzerland, I am back. Do you bless my approach above ?
Thanks and Regards
Nitin Harish
解決済! 解決策の投稿を見る。
Hi, Nitin
You can find block diagram as below. So you can set SIM_SOPT2[RTCCLKOUTSEL] = 1 and RTC_CR[CLK0] = 1.
Best Regards
Paul
Hi, Nitin
You can find block diagram as below. So you can set SIM_SOPT2[RTCCLKOUTSEL] = 1 and RTC_CR[CLK0] = 1.
Best Regards
Paul
I did follow from the exact same source.
Thanks for the confirmation.
My processor is :k64fn1m0vmd12