How can I help to port KL05 in MCUXpresso?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I help to port KL05 in MCUXpresso?

912 次查看
matheus_pinto1
Contributor II

Hello everbody,

 

As commented in this topic https://community.nxp.com/t5/Kinetis-Microcontrollers/mcuxpresso-for-KL05/td-p/787156, the KL05Z microcontroller doesn't have support of MCUXpresso SDK, and so, it can't be used in MCUXpresso IDE.

I like the FRDM-KL05Z board because: it is simple to use in an "embedded system" course; it is ARM based; it have an embed programmer; it is cheap to buy in Brazil (compared to other similar boards) and; I have many of these boards!

On the other hand, I like to use the "Open Pin" tool and, mainly, the "Open Clocks" tool because it makes teaching the microcontroller much easier.

I saw in the previous topic that it is a market issue to update the KL05Z for use in MCUXPresso. But, my question is: is it possible for me, as a customer, to help with the portability of the KL05Z to use the "Open pins" and "Open clocks" tools?

 

Thanks in advance.

标签 (1)
标记 (2)
0 项奖励
回复
0 回复数