Hello community. just received a kwikstik-40 and am unable to charge the battery

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hello community. just received a kwikstik-40 and am unable to charge the battery

460件の閲覧回数
jeffpurcell
Contributor I

Hello community.  just received a kwikstik-40 and am unable to charge the battery via USB. It powers up and runs while connected to USB but even after 5 hours it only shows 1 bar of charge and not enough to power up on the battery.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

380件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Jeff

As you can find, there is a ON/OFF switch on another side of Kwikstik_K40. Did you turn it on when you want to use this board?

If yes, there is still no 3.3V power. I think you need to check if battery still has energy.

Hope my reply can help you. Thanks.

Best Regards

Paul

0 件の賞賛
返信