Freescale Kinetis K70 MCU: FPU Demo

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Freescale Kinetis K70 MCU: FPU Demo

Freescale Kinetis K70 MCU: FPU Demo

The Kinetis K70 MCU family includes 512KB-1MB of flash memory, a single precision floating point unit, Graphic LCD Controller, IEEE 1588 Ethernet, full- and high-speed USB 2.0 On-The-Go with device charge detect, hardware encryption, tamper detection capabilities and a NAND flash controller. 256-pin devices include a DRAM controller for system expansion. The Kinetis K70 family is available in 196 and 256 pin MAPBGA packages.

For more information visit www.freescale.com/kinetis

标签 (1)
标记 (3)
无评分
版本历史
最后更新:
‎09-09-2012 03:01 PM
更新人: