FRDM-KW40Z SPI Port to Shield Connector Errata

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KW40Z SPI Port to Shield Connector Errata

384件の閲覧回数
marks
Contributor IV

Hello, Like to report some errata on the FRDM-KW40Z found by one of our customers. The blue text on the nets SW3 and SW4 that connects to the J1 shield connector on page 5 is wrong. Resulting in the SPI1 port clock and chip select lines being swapped on a custom board they built to mate to the Freedom board.

Net SW4, J1-10 on sheet 5 labled as PTA19/TSIO_CH13/SPI1_PCS0 but connects to PTA18 on the KW40

Net SW3, J1-12 on sheet 5 labled as  PTA18/TSIO_CH12/SPI1_SCK but connects to PTA19 on the KW40

I believe the problem is that the text in red is what the schematic capture tool uses to connect the nets. And the text in blue is supposed to be helpful “comments” and is wrong in this case. How is errata like this is documented on development boards? Maybe this is the first reported errata. Is there an errata document that is created and put under the "Documentation" tab?

Schematics for the FRDM-KW40Z are here:

FRDM-KW40Z|Freedom Development Platform|Kinetis MCU|NXP

Thanks!

Mark

0 件の賞賛
1 返信

259件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

I double checked the issue you mentioned, you are correct that we had the error for the two signal's connector. We are sorry that we do not have an official document errata at present. Anyway, I will report this issue to our document team and it will been addressed with some record. Thanks for reporeted the issue to us.

0 件の賞賛