FRDM-KE02Z40M board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KE02Z40M board

419件の閲覧回数
Circuit_Man
Contributor I

Hi NXP,

I have the FRDM-KE02Z40M board and I was told by another NXP rep that I should use MCUXpresso with this board, but I couldn't find my board as one of the targets, when I opened MCUXpresso. How can I add my board as a target in MCUXpresso or was it a mistake to install this IDE? And should I install CodeWarrior now, although it is being phased out?

0 件の賞賛
1 返信

414件の閲覧回数
myke_predko
Senior Contributor III

Hey @Circuit_Man 

You have to load the SDK for your Freedom board.  

You're going to MCUXpresso SDK Builder and select your Freedom board to build the SDK and download it.  When you have it on your PC, drag and drop it into the "Installed SDK" window in MCUXpresso.  

It's actually quite easy to do.  

0 件の賞賛