FRDM-KE02Z40M board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-KE02Z40M board

423 次查看
Circuit_Man
Contributor I

Hi NXP,

I have the FRDM-KE02Z40M board and I was told by another NXP rep that I should use MCUXpresso with this board, but I couldn't find my board as one of the targets, when I opened MCUXpresso. How can I add my board as a target in MCUXpresso or was it a mistake to install this IDE? And should I install CodeWarrior now, although it is being phased out?

0 项奖励
1 回复

418 次查看
myke_predko
Senior Contributor III

Hey @Circuit_Man 

You have to load the SDK for your Freedom board.  

You're going to MCUXpresso SDK Builder and select your Freedom board to build the SDK and download it.  When you have it on your PC, drag and drop it into the "Installed SDK" window in MCUXpresso.  

It's actually quite easy to do.  

0 项奖励