FRDM-KE02Z40M board powered with 120V wall adapter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KE02Z40M board powered with 120V wall adapter

543 Views
Circuit_Man
Contributor I

Hi Community,

I am interested in purchasing the FRDM-KE02Z40M development board, but I would like to power it from a 120V wall adapter. The reason is that I want to test the board as standalone, not connected to a PC. If this board can be powered from 120V, how do I indicate that I need a barrel connector on the board and also a wall adapter, so that when I receive it, it is ready to go. The description of this board states that it can be powered with an "External source power supply."

Thanks.

Labels (1)
0 Kudos
Reply
2 Replies

540 Views
mjbcswitzerland
Specialist V

Hi

You can power the board via USB cable from a standard USB charger (eg. as used to charge a smart phone, plugged into 120VAC). Also you can power it for a USB power pack (although they don't always turn on when the current is low and it may be necessary to load it with a parallel resistor).

Regards

Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or product development requirements

 

0 Kudos
Reply

534 Views
Circuit_Man
Contributor I

Thanks, Mark.

0 Kudos
Reply