FRDM-K64F freedom develpment board as a guideline for a new PCB. With this design a 50MHz clock is generated by the RMII Ethernet PHY and routed to the EXTAL0 (pin 50) of the K64 cpu. Of interest, the FRDM-K64F Rev E3 schematics show the XTAL0 output (pi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K64F freedom develpment board as a guideline for a new PCB. With this design a 50MHz clock is generated by the RMII Ethernet PHY and routed to the EXTAL0 (pin 50) of the K64 cpu. Of interest, the FRDM-K64F Rev E3 schematics show the XTAL0 output (pi

440件の閲覧回数
davidolsen
Contributor I

We are using the design for the FRDM-K64F freedom development board as a guideline for a new PCB. With this design a 50MHz clock is generated by the RMII Ethernet PHY and routed to the EXTAL0 (pin 50) of the K64 cpu. Of interest, the FRDM-K64F Rev E3 schematics show the XTAL0 output (pin 51) connected to GND thru a 0-ohm resistor (R74) via XTAL_K64_MAIN. When using an external clock, normally you leave the XTAL output unconnected. Why is this output connected to ground?


Thanks

0 件の賞賛
1 返信

273件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi David OLSEN,

    When you use the external reference clock as the clock source, not the external crystal, then you won't use the OSC module, XTAL0 is none used pin, it is better to connect to the ground, just the recommend design.

   The clocking diagram can help you to understand it.

   55.jpg

Wish it helps you!

If you still have question, please contact me!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛