Errata ERR050181 of Mask Set Errata for Mask 1N79P, Rev. 11Jan2022

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Errata ERR050181 of Mask Set Errata for Mask 1N79P, Rev. 11Jan2022

544件の閲覧回数
aporvasrivastava
Contributor I

Hi Team,

We are using MKE18F512VLH16 controller for our program. We have configured LPIT channel 1 and channel 0 in chain mode to measure the time (64-bit). Since we do not need any interrupt for these channel, interrupt is disabled for both channel. We are reading CVAL of the both channel to measure the time between two points or to add particular delay.

As per errata ERR050181 reading CVAL does not give correct value, so I have some questions as below to mitigate the issue.

1. Does CVAL reading always give incorrect value or issue is intermittent. If so, what is probability of it's occurrence.

2. As per mitigation provided in errata, CVAL should be read during an LPIT interrupt service routine, but for our program, interrupt is not required so it is disabled. Is there any other mitigation approach available ? 

 

ラベル(1)
0 件の賞賛
1 返信

539件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry for the inconvenience we bring you!
Please refer the discussion here: Tolerance of LPIT CVAL (Current timer value)

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛