Processor Expert has a Flash component which I used for the freedom board. I am able to successfully execute the Read Method. I can successfully execute the Write Method, but only once. If I try to write the 2nd time at the same memory location, it fails. It seems this is because the Write method does not Erase before writing.
I tried to execute the Erase and EraseBlock Method, but it did not work. It seems the "safe launch and wait" property of the Flash component prevented me from using the Erase Methods. Has anyone been able to use the Erase/EraseBlock Methods? If yes, can you please post some sample code, similar to sample code for Write and Read Methods examples given in the "Typical Usage" section of the Flash Component Help documentation.
Hi there, i want to store some data to the flash, but i don't know how to do it, i use cw 10.5 and set up of user memory areas is grey, and it doesn't have the FLASH1_GetOperationStatus function.and what should I send to the FLASH1Pointer parameter?
I found that you must erase a block size equivalent to the minimum block size of the processor. Trying to erase a smaller amount gives an error. This sounds sensible, though the comment in the PE definition of FLASH1_Erase() is not clear about this.
This works:
// don't try to erase 64 bytes!
//OpStatus = FLASH1_Erase(FLASH1Pointer, 0x1F000, sizeof(savedData));
OpStatus = FLASH1_Erase(FLASH1Pointer, 0x1F000, FLASH1_ERASABLE_UNIT_SIZE);
if (OpStatus != ERR_OK){
printf("Erase error. Status code is: %02x\n", OpStatus);
break;
}
How did you write the flash with longword? I am trying to write. buy I am confused about FCCOB 1:3 registers Flash address. I know the flash address ranges from 0x0000_0000 - 0x07FF_FFFF. which is 128K byte. how come FCCOB 1-3 registers only specify flash adress from 0 - 23 bits? supposed to be 0 -26 bits, right?
Hi Luis:
I implemented your code and it worked fine, but using the same code under FreeRtos, after erase operation I got the message :
No source available for "0xFFFFFFFE (0xFFFFFFFE)() "
I also tried disable interruptions during this operation but it didn't worked fine.
Do You have any suggestion ?
Thanks
Hello,
First, you have to reserve some Flash pages for data storage. Do that in the CPU Build Options, Reduce the Flash for code, for example :
Then, configure those pages to be used by Flash component:
Then, enable the Flash methods you need:
Now, you can save the data in the code:
Read:
FLASH1_Read(FLASH1Pointer,0x1F000, &savedData.red, sizeof(savedData));
do {
FLASH1_Main(FLASH1Pointer);
OpStatus = FLASH1_GetOperationStatus(FLASH1Pointer);
} while (!((OpStatus == LDD_FLASH_IDLE) | (OpStatus == LDD_FLASH_FAILED)));
Erase one page, in case is not 0xFF the locations to write:
FLASH1_Erase(FLASH1Pointer, 0x1F000, 1024);
do {
FLASH1_Main(FLASH1Pointer);
OpStatus = FLASH1_GetOperationStatus(FLASH1Pointer);
} while (!((OpStatus == LDD_FLASH_IDLE) | (OpStatus == LDD_FLASH_FAILED)));
And then write the data in Flash:
FLASH1_Write(FLASH1Pointer, FromPtr, 0x1F000, Size);
do {
FLASH1_Main(FLASH1Pointer);
OpStatus = FLASH1_GetOperationStatus(FLASH1Pointer);
} while (!((OpStatus == LDD_FLASH_IDLE) | (OpStatus == LDD_FLASH_FAILED)));
I hope this helps,
Luis