Does CW10.1 supports Kinetis K53

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does CW10.1 supports Kinetis K53

1,309件の閲覧回数
bhaskar_naik
Contributor I

We are unable to download the code to K53 tower module. It always gives following error 

 

"fl::target -lc "hvac_twrk53n512_Int_Flash_Debug_PEOSJTAG"
fl::target -b 0x20000000 0x10000
fl::target -v on -l off -ie on -i "D:/Program Files/Freescale/Freescale MQX 3.7/lib/twrk53n512.cw10/bsp/dbg/init_kinetis.tcl" -p MK53N512CMD100
 
Error: no such processor "MK53N512CMD100"

 

 

 

If I try to select the processor type in configuration, it does not list K50 series?

I have already applied patch for Kinetis K53.

 

IDE  version: CW10.1 with all the updates

Target : TWR K53N512

 

Any help will be appreciated..

0 件の賞賛
返信
2 返答(返信)

1,055件の閲覧回数
MikeRC
Contributor III

One place to start is I believe you have the TWR_K60N512.  Try that processor.

I'm not sure where the K53 is coming from, sounds like you might have to remove and re-install MQX 3.7 as well.

Also, make sure you have all the patches installed for MQX 3.7

0 件の賞賛
返信

1,055件の閲覧回数
bhaskar_naik
Contributor I

Yes it works with K60.

Currently IAR IDE is supported for K53. I could download the code using IAR IDE.

CW10 patch for K53 tower module is yet to be released.

0 件の賞賛
返信