Differential Input and Output voltage of DDR and USB Controller of MK70FN1M0VMJ12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Differential Input and Output voltage of DDR and USB Controller of MK70FN1M0VMJ12

596 Views
puspamnayak
Contributor III


Hi

Greetings for the day

Request you to let me know about  the exact values of Differential input volatge VID (min, max) and Differential output voltage VOD (min, max) of DDR signals and USB signals of part no. MK70FN1M0VMJ12

Kindly reply ASAP

Thanks in advance

Best Regards

Puspam Nayak

Tags (1)
0 Kudos
Reply
2 Replies

465 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi PUSPAM NAYAK,

DDR controller are compliant to DDR2 SDRAM spec, and USB controller are compliant to USB 2.0 spec, so you may find data from www.jedec.org and www.usb.org.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

465 Views
puspamnayak
Contributor III

Hi Kan,

Thanks for the information. I will refer the same

Warm regards,

Puspam

0 Kudos
Reply