Hi,I try to start MQX 4.1.1 on FRDM64F platform with IRC48M. According to the AN4905 documentation,do the relevant configuration. but each time OS is stopped in PBE mode, wait until external reference clock is selected as MCG output. I am very upset, please expert help, thank you!
According to document, I use PE to do the configuration, But still not solve the problem.
PE configuration as follows:
Add the following content in the _bsp_initialize_hardware(void) functions:
/* SIM_CLKDIV2:USBDIV = 0, USBFRAC = 0*/
SIM_CLKDIV2 = (uint32_t)0x0UL;
/* Configure USB to be clocked from IRC 48MHZ */
SIM_SOPT2_REG(SIM_BASE_PTR) |= SIM_SOPT2_USBSRC_MASK | SIM_SOPT2_PLLFLLSEL(3);
/*Enable USB-OTG IP clocking */
SIM_SCGC4_REG(SIM_BASE_PTR) |= SIM_SCGC4_USBOTG_MASK;
/* Enable IRC48MHZ for USB module*/
USB0_CLK_RECOVER_IRC_EN = 0x03;
/* MCG_C7: OSCSEL = 10*/
MCG_C7 |= 0x2u;
/* USB_CLK_RECOVER_CTRL: CLOCK_RECOVER_EN = 1*/
USB0_CLK_RECOVER_CTRL |= ( 1UL << 7);
The problem is OS stay on the PBE patterns, wait until external reference clock is selected as MCG output or wait until PLL is locked.
Thank you!
已解决! 转到解答。
Hi John Baker!
I use system_MK64F12.c debug bare board program, stop in exception hardfault.
I doubt MK64F cannot work without external crystals and only IRC48M cases. The official did not provide a demo program with IRC48M on K64,K63 or K24 family devices.
Thank you!
Qingjun Wang