Beginner looking for help with CodeWarrior and Freescale TWR-K70F120M

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Beginner looking for help with CodeWarrior and Freescale TWR-K70F120M

421 次查看
benjaminbergand
Contributor I

Hi, I am looking for a useful tutorial that explains how CodeWarrior interfaces with the Freescale TWR-K70F120M. I have never worked with this environment before and cannot find any useful resources that explains initializing hardware, using flash programming, etc. Any help would be appreciated!

0 项奖励
1 回复

348 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Benjamin,

- About how to use the CW develop the board , there is quick start about CW under the installation directory :

....\Freescale\CW MCU v10.6\MCU\Help\Quick_Start_for_Microcontrollers.pdf

or "Quick_Start_for_Microcontrollers.pdf\Targeting_Microcontrollers.pdf"

- About the demo code about TWR-K70,  you can download here :

Kinetis K70 120 MHz Tower System Module|Freescale

pastedImage_1.png

Hope it helps


Have a great day,

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励