I am using a K64F in MAPBGA 144 package and have a debug header wired to the MCU requiring routing of the TRACE_CLKOUT signal to pin D3. The K64 Sub-Family Data Sheet indicates in the Pinout chapter that pin D3 can be routed for TRACE_CLKOUT using the ALT5 mux configuration. By contrast, I noticed that in the MCUXpresso Config Tools > Pins view > Peripheral Signals tab, the SIM > CLKOUT signal only has two pins available to it: A11 and J7. This is in direct conflict with the K64 Sub-Family Data Sheet. Which information is accurate?
已解决! 转到解答。
Hi,
The D3 is not belong to the SIM. It belongs to TPIU. You will find D3 under the peripheral TPIU.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
The D3 is not belong to the SIM. It belongs to TPIU. You will find D3 under the peripheral TPIU.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------