Greetings everyone,
I am stuck - On a partitioning problem that continually resets.
TARGET HARDWARE: MK12DX256VLF5
TOOL: IAR (J-Link Debugger)
I use the following code which I got directly from Freescale:
main()
{
...
printf(" Checking For *NV Memory Partition...\r\n");
if (partition_flash(EEPROM_128_128, DFLASH_SIZE_0)) // passed values are 0x36 and 0x08
printf(" **New Flex Memory Partition\r\n");
else
printf(" >>Device Already Partitioned\r\n");
...
}
bool_t partition_flash(uint8_t EEProm_size, uint8_t DFlash_size)
{
/* Test to make sure the device is not already partitioned. If it
* is already partitioned, then return with no action performed.
*/
if ((SIM_FCFG1 & SIM_FCFG1_DEPART(0x0F)) != 0x00000F00)
return(FALSE);
/* Write the FCCOB registers */
FTFL_FCCOB0 = FTFL_FCCOB0_CCOBn(0x80); // Selects the PGMPART command
FTFL_FCCOB1 = 0x00;
FTFL_FCCOB2 = 0x00;
FTFL_FCCOB3 = 0x00;
/* FCCOB4 is written with the code for the subsystem sizes (eeprom_size define) */
FTFL_FCCOB4 = EEProm_size;
/* FFCOB5 is written with the code for the Dflash size (dflash_size define) */
FTFL_FCCOB5 = DFlash_size;
/* All required FCCOBx registers are written, so launch the command */
FTFL_FSTAT = FTFL_FSTAT_CCIF_MASK;
/* Wait for the command to complete */
while((FTFL_FSTAT & FTFL_FSTAT_CCIF_MASK) == 0x00);
return(TRUE);
}
If the device is blank and I run the partition code it resets (Core Lockup Event) at the execute partiton command (bold line) every time. If I set a break point at that line (bold line) then run it resets, but if I set a break point (at the bold line) then step one line it works. the registers before the execution of the command look (I think) as they should...
FTFL_FSTAT: 0x80
FTFL_FCNFG: 0x02
FTFL_FSEC: 0xFE
FTFL_FOPT: 0xFF
FTFL_FCCOB0: 0x80
FTFL_FCCOB1: 0x00
FTFL_FCCOB2: 0x00
FTFL_FCCOB3: 0x00
FTFL_FCCOB4: 0x36
FTFL_FCCOB5: 0x08
FTFL_FCCOB6: 0x00
FTFL_FCCOB7: 0x00
FTFL_FCCOB8: 0x00
FTFL_FCCOB9: 0x00
FTFL_FCCOBA: 0x00
FTFL_FCCOBB: 0x00
FTFL_FPROT0: 0xFF
FTFL_FPROT1: 0xFF
FTFL_FPROT2: 0xFF
FTFL_FPROT3: 0xFF
FTFL_FEPROT: 0xFF
FTFL_FDPROT: 0xFF
I have also insered delays before the command execution (upto 1s) thinking it was timing related with no change of result. Thinking it was unique to the J-Link debugger I loaded the code to the target and there it also resets.
Any help on this would be great...
Thanks,
Hab
解決済! 解決策の投稿を見る。
SOLUTION... FUNCTION NOTES ARE IMPORTANT
/*************************************************************************
* Function Name: partition_flash
* Parameters: uint8_t, uint8_t
* Return: bool_t
* NOTE: This function should be called before IRQs (espcially timers) are set to run
* as the partitioning process must not be interuppted
* NOTE: Flex NV Memory can be divided into EFlash (EE NV), DFlash Space or a combination
* of the two. The max EE space is 4KB. The smaller the DFlash the longer the life of the EE NV
* See Freescale App Note AN4282 for more information
*
* Description: Partition flash routine. This function can be used to setup
* the flash for enhanced EEPROM operation. In order to guarantee
* the eEE endurance the partition command should only be used one
* time (re-partitioning in a different configuration will erase
* wear-leveling data, so endurance can no longer be guaranteed).
* This function will test to make sure the flash has not been
* partitioned already.
*
* Why: The very first time firmware runs it must partition the memory for use.
* By partitioning the memory NV EE memory is created within the micro.
*
* STEP 1: Check if the device was previously partitioned
* STEP 2: Clear Status Register Flags and Load for the FCMD Program Partition Command
* STEP 3: Execute the command and return when done
*************************************************************************/
bool_t partition_flash(uint8_t EEPROM_Size, uint8_t DFlash_Size)
{
// STEP 1:
// CHECK FOR PREVIOUS PARTITION AND RETURN FALSE IF IT WAS
if ((SIM_FCFG1 & SIM_FCFG1_DEPART(0x0F)) != 0x00000F00)
return(FALSE);
// STEP 2:
// CLEAR RDCOLERR, ACCERR AND FPVIOL FLAGS OF THE STATUS REGISTER
FTFL_FSTAT = (FTFL_FSTAT_RDCOLERR_MASK | FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK);
// WRITE THE VALUES TO LOAD THE FCMD FOR PROGRAM PARTITION
FTFL_FCCOB0 = FTFL_FCCOB0_CCOBn(FCMD_PROGRAM_PARTITION);
FTFL_FCCOB1 = 0x00;
FTFL_FCCOB2 = 0x00;
FTFL_FCCOB3 = 0x00;
FTFL_FCCOB4 = EEPROM_Size;
FTFL_FCCOB5 = DFlash_Size;
// STEP 3:
// EXECUTE THE FCMD COMMAND AND RETURN WHEN DONE
FTFL_FSTAT = FTFL_FSTAT_CCIF_MASK;
while((FTFL_FSTAT & FTFL_FSTAT_CCIF_MASK) == 0x00);
return(TRUE);
} // END OF partition_flash
SOLUTION... FUNCTION NOTES ARE IMPORTANT
/*************************************************************************
* Function Name: partition_flash
* Parameters: uint8_t, uint8_t
* Return: bool_t
* NOTE: This function should be called before IRQs (espcially timers) are set to run
* as the partitioning process must not be interuppted
* NOTE: Flex NV Memory can be divided into EFlash (EE NV), DFlash Space or a combination
* of the two. The max EE space is 4KB. The smaller the DFlash the longer the life of the EE NV
* See Freescale App Note AN4282 for more information
*
* Description: Partition flash routine. This function can be used to setup
* the flash for enhanced EEPROM operation. In order to guarantee
* the eEE endurance the partition command should only be used one
* time (re-partitioning in a different configuration will erase
* wear-leveling data, so endurance can no longer be guaranteed).
* This function will test to make sure the flash has not been
* partitioned already.
*
* Why: The very first time firmware runs it must partition the memory for use.
* By partitioning the memory NV EE memory is created within the micro.
*
* STEP 1: Check if the device was previously partitioned
* STEP 2: Clear Status Register Flags and Load for the FCMD Program Partition Command
* STEP 3: Execute the command and return when done
*************************************************************************/
bool_t partition_flash(uint8_t EEPROM_Size, uint8_t DFlash_Size)
{
// STEP 1:
// CHECK FOR PREVIOUS PARTITION AND RETURN FALSE IF IT WAS
if ((SIM_FCFG1 & SIM_FCFG1_DEPART(0x0F)) != 0x00000F00)
return(FALSE);
// STEP 2:
// CLEAR RDCOLERR, ACCERR AND FPVIOL FLAGS OF THE STATUS REGISTER
FTFL_FSTAT = (FTFL_FSTAT_RDCOLERR_MASK | FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK);
// WRITE THE VALUES TO LOAD THE FCMD FOR PROGRAM PARTITION
FTFL_FCCOB0 = FTFL_FCCOB0_CCOBn(FCMD_PROGRAM_PARTITION);
FTFL_FCCOB1 = 0x00;
FTFL_FCCOB2 = 0x00;
FTFL_FCCOB3 = 0x00;
FTFL_FCCOB4 = EEPROM_Size;
FTFL_FCCOB5 = DFlash_Size;
// STEP 3:
// EXECUTE THE FCMD COMMAND AND RETURN WHEN DONE
FTFL_FSTAT = FTFL_FSTAT_CCIF_MASK;
while((FTFL_FSTAT & FTFL_FSTAT_CCIF_MASK) == 0x00);
return(TRUE);
} // END OF partition_flash
Hi,
Are you able to fix reset issue.
Can you tell me how to overcome reset issue.
I am using SK32K144/SK32K148
Regards,
Sudarshan