Are the A/D pins on the K70 MCU 5V tolerant?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Are the A/D pins on the K70 MCU 5V tolerant?

415 次查看
ahuq
Contributor I

The VDD on my MK70 CPU is at 3.3V and I am using using some of my GPIO pins as A/D . I have several op amps that are tied to my A/D pins for reading the voltages. My max voltage from op amp is 5V and I would like to know if my A/D on my MK CPU is 5V tolerrant.

0 项奖励
2 回复数

315 次查看
cutworth
NXP Employee
NXP Employee

Hi,

You can refer the voltage and current rating spec in K70 DS.

pastedImage_0.png

The digital I/Os are 5V tolerant, this also includes the GPIOs with AD functions. For analog only pins, it's not 5V tolerant.

But for your question, you want to know if ADC is 5V tolerant or just the AD pins. Even the GPIO pins are 5V tolerant, when you input a voltage over VREFH of ADC, it will convert to 0xFFFF for 16bit mode. Is this meaning in your application? You do not want to add resistor divider for ADC inputs?

Hao

0 项奖励

315 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Al-hamra Huq,

      Please refer to the K70 datasheet:

69.jpg

   You can see, the ADC input voltage can't exceed 31*/32 VREFH when in 16bit differential mode, and all the other modes, the ADC input voltage can't exceed VREFH.

   The max Value of VREFH is VDDA, it is 3.6V.

   So, the ADC input pin is not the 5V tolerant pin, please take care!

Wish it helps you!

If you still have question, please let me know!

Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励