I am using a KEA128 uC with Cyclone FX debugger. I was able to configure RTC and saw RTC_CNT kept running. RTC_SC_RTIF flag also got set periodically. However, RTC_IRQHandler() never got called. I found a RTC example from TRK-KEA128_LABTS5/ where it has a routine called Enable_Interrupt() and NVIC_ICPR and NVIC_ISER are set accordingly. Is this enabling routine still required? Since, both of them are no longer defined in SKEAZ1284.h coming with the lastest S32 Design Studio for ARM. Please advise. Thanks!
解決済! 解決策の投稿を見る。
Hi Shangpin,
Please download the FRDM-KEAZ Freedom Evaluation Board – QSP (REV 8 ) .
Then refer the FRDM_KEA128_RTC example. NVIC_ISER is needed to enable interrupt.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Shangpin,
Please download the FRDM-KEAZ Freedom Evaluation Board – QSP (REV 8 ) .
Then refer the FRDM_KEA128_RTC example. NVIC_ISER is needed to enable interrupt.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Exactly the answer I was looking for! Thanks for the pointer to the up-to-date example code. They are very helpful.