Are FRDM-KW41Z drivers compatible with Windows 10? If not, when are they expected to be?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Are FRDM-KW41Z drivers compatible with Windows 10? If not, when are they expected to be?

849 次查看
morechnikov
Contributor III

Same question applies for the other FRDM-KW boards (KW20Z, KW30Z, KW40Z).

标签 (1)
2 回复数

539 次查看
miduo
NXP Employee
NXP Employee

Hi,

I am thinking that what you mean " support" should be the IDE that the board used with. There are two IDEs we provide to support FRDM-KW41Z, IAR EWARM and NXP KDS. Both are work with Win 10.

539 次查看
morechnikov
Contributor III

Hello,

Thanks for the response. Previously, I worked with the FRDM-KL25Z and KE02Z. Their main issue is that Windows 10 does not detect them, no USB storage for firmware and no COM port for programming. Even after OpenSDA and P&E Micro drivers are installed from the internet. The KDS IDE works fine, but it can't detect the COM Port (OpenSDA) interface (neither can Device Manager). My question is in regards to the KW41Z's, and newer models', plug-and-play and/or P&E Micro/OpenSDA driver functionality, specifically in the Windows 10 environment. I apologize for any confusion.

0 项奖励