Hi !
I would like to disable accesses from untrusted masters to memory and peripheral area for K82 MCU.
Only Master0 and 1 can have access to enabled areas.
I have configured MPU Regions in way when memory and peripheral area (0x40000000-0xFFFFFFFF) give acess for Master0 only. In Region0 i have disabled all Masters and only Master1 is remains.
I undestand that if address range is not covered by MPU region, any master can access to it.
Is this true ?
After that I have disabled all other masters for read/write in AIPSx-MPRA registers for limit access to peripherals.
Does it really need, MPU already covered peripheral area and access from masters disabled there already ?
MPU of K82 covers some or all peripheral area but from documentaion is not so clear what exact address ranges are
covered by MPU ?
After that I have checked AIPSx-PACRx register and see posibility to disable access from untrasted master on per peripheral level, one by one.
Does it is really need ? Can MPRA or MPU filter all untrasted masters already ?
E.g what minimal setting required for protect all memory and peripheral areas from other masters than 1 &2 ?
Regards,
Eugene
已解决! 转到解答。
Hi,
peripheral space(from 0x40000000) is not protected by MPU. It is protected by AIPS-Lite itself. MPU protects SRAM, QSPI, BOOT ROM and Flash, SDRAM, Fexbus. AIPS-Lite protects peripheral space. If address range is not covered by MPU region, any master can access to it.
Regards
Jing
Hi,
peripheral space(from 0x40000000) is not protected by MPU. It is protected by AIPS-Lite itself. MPU protects SRAM, QSPI, BOOT ROM and Flash, SDRAM, Fexbus. AIPS-Lite protects peripheral space. If address range is not covered by MPU region, any master can access to it.
Regards
Jing