ADC Reference Options on KL17/KL27 32/36pin package

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC Reference Options on KL17/KL27 32/36pin package

ADC Reference Options on KL17/KL27 32/36pin package

Many customers reported that their ADC function works on FRDM-KL27Z board but meet issue on their own board. We need to pay attention to the difference between the ADC reference voltages of different packages (on board MKL27Z64VLH4 is 64LQFP package).

This tip introduce the ADC Reference Options on KL17/KL27 32/36pin package

Part number involved:

32-pins36-pins
MKL17Z32VFM4MKL17Z32VDA4
MKL17Z64VFM4MKL17Z64VDA4
MKL27Z32VFM4MKL27Z32VDA4
MKL27Z64VFM4MKL27Z64VDA4

PTE30/VREF_OUT- connected as the primary reference option on 36-pin and below packages

VDDA/VSSA - connected as the VALT reference option

24.1.5 ADC Reference Options.png 

ADCx_SC2[REFSEL] selects the voltage reference source used for conversions.

PTE30 VREF_OUT.png

 

About the primary reference option:

onchip 1.2V VREF or external reference voltage.png

  1. When on-chip 1.2V VREF is enabled, PTE30 pin must be used as VREF_OUT and has to be configured as an analog input, such as ADC0_SE23 (PORTE_PCR30[MUX] = 000).
    Notice: this pin needs to connect a capacitor to ground.
    PTE30 VREF_OUT.png 
  2. PTE30 can also be used as an external reference voltage input as long as PTE30 is configured as analog input and VREF module is disabled.
    It means you can connect external reference voltage to PTE30 pin and use it as ADC reference voltage. (For example 3.3V)

KL17P64M48SF2RM     Kinetis KL17: 48MHz Cortex-M0+ 32-64KB Flash (32-64pin) (REV 4.1)
KL27P64M48SF2RM     Kinetis KL27: 48MHz Cortex-M0+ 32-64KB Flash (32-64pin) (REV 4.1)

标签 (1)
100% 有帮助 (1/1)
版本历史
最后更新:
‎11-16-2018 01:08 AM
更新人: