能提供下MKE04Z128VLK4的库函数吗

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

能提供下MKE04Z128VLK4的库函数吗

Jump to solution
1,701 Views
旭余朱
Contributor III

你好,能提供下MKE04Z128VLK4的库函数吗?官网的库函数似乎只是针对开发板的,比如GPIO_Init(GPIO_Type *pGPIO, uint32_t u32PinMask, GPIO_PinConfigType sGpioType)中初始化也只能初始化部分端口。我用的是keil。

Labels (1)
0 Kudos
1 Solution
1,517 Views
kerryzhou
NXP TechSupport
NXP TechSupport

楼主你好!

关于MKE04Z128VLK4的库函数,你可以直接下官方的SDK。

https://mcuxpresso.nxp.com/en/select 

芯片你选择MKE04Z128VLK4,然后编译并下载对应的SDK包,如果需要MDK的,你IDE那边就选择MDK的,或者选择所有IDE的。

pastedImage_3.png

下载之后,虽然你的工程还是板子的,但是你打开:

SDK_2.7.0_MKE04Z128xxx4\devices\MKE04Z1284, 你还会发现有对应的驱动。

pastedImage_4.png

这样,对应具体的工程,你只需要把相关的文件用上面文件夹中的驱动更新下就可以了。

希望能帮到。

如果还有问题,欢迎继续交流!~

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

3 Replies
1,518 Views
kerryzhou
NXP TechSupport
NXP TechSupport

楼主你好!

关于MKE04Z128VLK4的库函数,你可以直接下官方的SDK。

https://mcuxpresso.nxp.com/en/select 

芯片你选择MKE04Z128VLK4,然后编译并下载对应的SDK包,如果需要MDK的,你IDE那边就选择MDK的,或者选择所有IDE的。

pastedImage_3.png

下载之后,虽然你的工程还是板子的,但是你打开:

SDK_2.7.0_MKE04Z128xxx4\devices\MKE04Z1284, 你还会发现有对应的驱动。

pastedImage_4.png

这样,对应具体的工程,你只需要把相关的文件用上面文件夹中的驱动更新下就可以了。

希望能帮到。

如果还有问题,欢迎继续交流!~

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,517 Views
旭余朱
Contributor III

谢谢拉

0 Kudos
1,517 Views
kerryzhou
NXP TechSupport
NXP TechSupport

不客气,如果还有问题,欢迎继续交流!

如果问题解决了,还请帮我标下正确答案,以示结贴,谢谢!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos