kenetis design studio 3.0 with Ksdk1.3 will not run debugger on K22F demo board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kenetis design studio 3.0 with Ksdk1.3 will not run debugger on K22F demo board

521件の閲覧回数
jeff_sylvester
Contributor I

I just installed KDS3.0 and SDK1.3 with demo Freeedom K22F  I went trough and did quick start guide, installing Jlink 2.1 on to OpenSDK,  and sucessfully get terminal program.  so went to Frdm-K22f page, and imported prosample projects into KDS and compile successfully, then go to debug, and get error, "Launching (project name) debug cmsisdap has encountered problem. 

"

An internal error occurred during: "Launching i2c_comm_mstr_frdmk22f debug cmsisdap".

ilg.gnuarmeclipse.debug.gdbjtag.dsf.GnuArmServicesFactory.<init>(Ljava/lang/String;Ljava/lang/String;)V"

 

this is probably some kind of set up or configuration error in the tool?

ラベル(1)
0 件の賞賛
1 返信

336件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Jeff,

If you loaded the JLink OpenSDA firmware to your board then you need to select the "GDB SEGGER J-Link Debugging" connection instead of the OpenOCD connection:

pastedImage_1.png

pastedImage_0.png

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛