Hi,
I have downloaded the FRDM-KL28 SDK and processor from mcuxpresso.nxp.com but when I open it there is nothing in the examples. Normally when you great new SDK2 project it will have boards > FRDM-KL28 Board > Examples > driver_examples.
While I understand the drivers are reasonably straight forward, for me its MUCH quicker to just get a working example and start from there (which is what i did with the KL27).
Where do I get the board examples? Did I do something wrong to not get all the examples, or demo applications?
Solved! Go to Solution.
Ok, I found them, the project wizard is either not working, or not supporting finding them int he folder. They're in the actual folder you just have to get them manually using add project or which ever method you use.
Ok, I found them, the project wizard is either not working, or not supporting finding them int he folder. They're in the actual folder you just have to get them manually using add project or which ever method you use.
I'm using MCUXpresso IDE 10.1.0, and it works for me:
What might be different on your side?
Erich
Thanks for that, I am using KDS. Should I be using this IDE instead? I have not been around this product for a while as I have been off working on on other projects.
Hi Carl,
yes, I recommend MCUXpresso IDE: it works very nicely with the SDK and has many extra features compared to KDS (which has been replaced by MCUXpresso IDE).
Erich