Hello,
My target is TWR-K64F120 +TWR-SER2, using KDS and FREERTOS, I've created a project which
is running OK and I can communicate over the serial link to a terminal using the DB9 connector on the SER2 board.
However I need to add SHELL to this project. I noticed that there is a shell folder in the SDK that I'm using.
I'm not certain how to integrate the files in the shell folder into my project.
Is there a tutorial for this?
Please even if someone has done this for a bare metal (without any OS) your input is very valuable.
Any help is greatly appreciated.
Thanks,
Koorosh Hajiani
Hi Koorosh,
I just asked a similar question and got an encouraging response. See my thread:
Can I easily extend FreeRTOS in the new Kinetis SDK v2.0?
Good luck!,
Peter