RTCESL problems with KV46 @ KDS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTCESL problems with KV46 @ KDS

656 Views
jirictibor
Contributor I

Hello people,

 

I would like to use the RTCESL library. I am using TWR-KV46 dev board in KDS with KSDK1.3.0_KV4xF_1.0.0 with Processor Expert support. I successfully included the libraries (MLIB, GFLIB), but when I use some function of the library in my code, after some time (few cycles) the processor got stuck in an unexpected place: XBARA_IQRHandler()... even if I've never used this component of periphery yet. You can see the image below.

194207_194207.pngpastedImage_1.png 

 

If you have any suggestions please tell me. Or if somebody needs more information please write me.

 

Thank you very much,

Jiri.

Original Attachment has been moved to: pwm_kv46.zip

0 Kudos
2 Replies

508 Views
jirictibor
Contributor I

Hello Alice,

OK i will try it, but i think that problem was, that it requires too many steps until it stuck so it is not possible to debug it step by step and wait for the stuck. But I am not sure, I will try it again and deeper.

But I have preliminary results, I've try it just now at KV31 board, but with SDK 2.2 and without PEx and it works. So it is too early to make a conclusion.

I will investigate it tomorrow.

Thanks for the support!

BR, Jiri.

0 Kudos

508 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jiri,

Please debug step by step or using breakpoinits to check when run to which code,

then it crash.

BR

Alice

0 Kudos