PE in KDS 3.0.0 does not set open drain mode for I2C pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PE in KDS 3.0.0 does not set open drain mode for I2C pins

787件の閲覧回数
alexfeinman
Contributor III

In the code generated by KDS 3.0.0 for I2C initialization there is no call to PORT_HAL_SetOpenDrainCmd. As a result the I2C pins end up in push/pull mode which is against the I2C spec and causes no end of problems with devices that are not strong enough to overcome weak pull-up on Kinetis devices (an example would be Toshiba TC358765 DSI to LVDS chip). Am I missing something here?

 

 

Here is the code generated by KDS 2.0.0 (in the pin_mux.c)

void pin_mux_I2C(uint32_t instance)

{

  switch(instance) {   

    case 0:                             /* I2C0 */

      /* PORTB_PCR2 */

      PORT_HAL_SetMuxMode(PORTB_BASE,0u,kPortMuxAlt2);

      PORT_HAL_SetOpenDrainCmd(PORTB_BASE,0u,true);

      /* PORTB_PCR3 */

      PORT_HAL_SetMuxMode(PORTB_BASE,1u,kPortMuxAlt2);

      PORT_HAL_SetOpenDrainCmd(PORTB_BASE,1u,true);

      break;

    case 1:                             /* I2C1 */

      /* PORTC_PCR10 */

      PORT_HAL_SetMuxMode(PORTE_BASE,0u,kPortMuxAlt6);

      PORT_HAL_SetOpenDrainCmd(PORTE_BASE,0u,true);

      /* PORTC_PCR11 */

      PORT_HAL_SetMuxMode(PORTE_BASE,1u,kPortMuxAlt6);

      PORT_HAL_SetOpenDrainCmd(PORTE_BASE,1u,true);

      break;

    default:

      break;

  }

}

 

And here is what I get with KDS 3.0.0:

void init_i2c_pins(uint32_t instance)

{

  switch(instance) {   

    case I2C0_IDX:                      /* I2C0_IDX */

      /* Affects PORTB_PCR0 register */

      PORT_HAL_SetMuxMode(PORTB,0UL,kPortMuxAlt2);

      /* Affects PORTB_PCR1 register */

      PORT_HAL_SetMuxMode(PORTB,1UL,kPortMuxAlt2);

      break;

    case I2C1_IDX:                      /* I2C1_IDX */

      /* Affects PORTE_PCR1 register */

      PORT_HAL_SetMuxMode(PORTE,1UL,kPortMuxAlt6);

      /* Affects PORTE_PCR0 register */

      PORT_HAL_SetMuxMode(PORTE,0UL,kPortMuxAlt6);

      break;

    default:

      break;

  }

}

Quite obviously, the latter is wrong. From the I2C specification:

"The output stages of devices connected to the bus

must have an open-drain or open-collector to perform the

wired-AND function"

ラベル(1)
0 件の賞賛
2 返答(返信)

486件の閲覧回数
Lukas_Heczko
NXP Employee
NXP Employee

Hi Alex,

what processor and Kinetis SDK you used?

Generally, you can enable an open drain in the PinSettings component where if you go to Functional Properties tab you can set all electric features of the pins. The code is then generated in pin mux function.

OpenDrainControl.png

Regards,

Lukas

0 件の賞賛

486件の閲覧回数
alexfeinman
Contributor III

MK26FN2M0. Yes, I can adjust the OD setting in the pinmux. The point is that I shouldn't have to and I didn't have to until KDS 3.0.0. The whole point of PE is to make correct things happen automatically. When configuring I2C it means selecting the correct alt setting and configuring open drain.

This is most definitely a bug