Using Linux 64 bit with Latest KDS
2 annoying bugs here wasting my time:
1. Go to help->search
type in CPU_ to search for all the valid cpu defines
hit GO,
pulls up 77 items.
Click on first item, KDS BLOWS UP and exits with no warning.
2. Compile a project under debug, loads and runs fine with PE multilink.
Compile release version of project, no errors
Try to flash project, multilink will not connect to target, sees mulitlink it, but won't connect.
I am ASSUMING it's because target is MK22FN1m0 and code is linked to MK22FN512.
So if this is the issue why is there no error message telling me it actually DID find it but it'snot what was expected. Why is there no forced override?
Ken
Hi Ken,
I am really sorry for your inconvenience. I reproduced the problem on clean Ubuntu 14.04. It is caused by segmentation fault in jvm. Are you able to upgrade to Ubuntu 16.04? Thank you.
Regards,
Michal
Michal,
I'm glad you see it too. No I can't upgrade at this time. 16.04 won't
run or fit on the machine it's on and I don't want to spend the time
messing with it. This is a total productivity time waster.
so what's causing the seg fault? Why is jvm broken here?
Again I must stress that any dev IDE built on java is garbage and not
maintainable long term. Once again eclipse has stuck it to me so I am
not going to continue to feed this monster.
thanks
Ken
Well of course you can't reproduce it. KDS for linux CLEARLY states it
was tested on 14.04 LTS, so if this is true it should work on this out
of the box with no mods. Don't know what version of java it comes with
it..shouldn't really matter. It shouldn't use ANY java, just the native
desktop environment,
which in this case is python for extras.
Your version probably has some different or updated libs not in 14.04.
So I'm, supposed to keep upgrading my workstation every time NXP puts
out a new release. I don't think so...
What I see happening here in the industry is TOO much focus on glitz and
marketing and TOO LITTLE attention to the actual tools used to do work.
This is a dev environment, It's expected it should compile,link load
programs, nothing more. By rights it should not ever have a net
connection or rely on the net for anything since in many company
environments security dictates no possible outside access to code source.
This is not an iphone and I for one am getting sick of every dev
environment looking like one.
Whoever is doing the planning is failing miserably, no cohesive overall
strategy.
Do you want to sell chips or play games? choose 1.
just my 2 cents
Ken
Hi Marek,
2 projects actually.
1. a modified bootloader based on boot code 2.0
2. custom project created in CW and moved to Kinetis.
Project 2 compiles and runs fine in debugger. If I make a release
version, it compiles but PE multilink FX won't flash it..seems to
complain about wrong cpu, which can't be right since it debugs fine. The
only real difference between these CPUs is the flash size, all things
being equal.
Project 1 compiles, won't run or flash. This is probably due to the fact
I modified it for the MK22FN1M0 part which is NOT in the 2.0 release and
something the PE is picking up doesn't match the CPU signature, this is
a guess??? The bootloader defines a CPU_xxx type in the project. I
changed this to what I thought was correct, but not sure if it is the
right word/spelling..Can't find a reference to what is legal here..this
should be so simple.
As I mention in last post I tried to find this in help but help crashed
the IDE. A little more investigation seems to indicate it doesn't like
some java crap on my machine...The Linux version clearly has some
install or setup bugs not being addressed, so I'm hoping I can get this
to work adequately enough to do the project.
Kinetis did upgrade the PE firmware when first attached, so I would
think everything is up to date here...
Thanks for the interest
Ken