Kinetics design studio project opening problem.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetics design studio project opening problem.

2,534 Views
akshaybhavsar
Contributor I

Hi,

I have installed kinetis Design studio.I have firmware for MK64FN1MOVLL12 controller.I cant open this project as i go to project ->open project.

0 Kudos
Reply
12 Replies

2,180 Views
akshaybhavsar
Contributor I

For 32 bit ubuntu

0 Kudos
Reply

2,180 Views
akshaybhavsar
Contributor I

So,which IDE I can use for MK64FN family controller

Regards,

Akshay.

0 Kudos
Reply

2,180 Views
sanketmeher
Contributor II

In dont find set up for 32 bit ubuntu OS.I could install it on 64-bit ubuntu.Please send me link to get IDE for 32 bit ubuntu.

Sincerely,

Regards,

Akshay.

2,180 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Unfortunately, for KDS for Linux, it only supports 64bit system.

There is no KDS version for 32bit ubuntu yet.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,180 Views
akshaybhavsar
Contributor I

I have installed it in windows.It worked for me.But i want to install it for ubuntu too.It generates tar.gz file.Dont know how to install this file.

Sincerely,

Regards,

Akshay.

0 Kudos
Reply

2,180 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

you don't need install chip sdk (for example SDK_2.2_FRDM-K64F) to your KDS as a patch. you just need discompress it to your local disk. then follow Getting Started with MCUXpresso SDK.pdf (under your chip sdk folder ) , chapter 5 Run a demo using Kinetis Design Studio IDE to work with it.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,180 Views
akshaybhavsar
Contributor I

It generates .tar.gz file.Kinetis IDE accept only .zip file

0 Kudos
Reply

2,180 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Please make sure you select Host OS as windows.

It's possible to get .tar.gz if you seclect Host OS as Linux.

see attached video.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,180 Views
akshaybhavsar
Contributor I

If we make new project there is option for selecting SDK.but how to select SDK for exhisting project.

0 Kudos
Reply

2,180 Views
akshaybhavsar
Contributor I

I have installed kinetis IDE.I have opened project successfully.I need to install SDK.Which SDK i need to install for MK64FN1MOVLL12 controller?

0 Kudos
Reply

2,180 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Please go to this url then follow the video to download SDK2.2.

Welcome to MCUXpresso | MCUXpresso Config Tools 

please note:

1. select the correct configuration for your target

2. make sure the sdk you download is built for KDS.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,180 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

the "project ->open project" feature works for a closed project inside "project explorer".

If you want to import another project into KDS IDE, use "File->import".

See attached video for what I am talking above. Hope this helps.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply