Hi,
when connecting to my target hardware (KV46F) through the PE GDB and OPENSDA a warning in the console occurs several times (see below): Warning 17927. Target MCU mismatch. Download performance limited. See http://www.pemicro.com/opensda/pe_tools.cfm for information on debugging external processors.
Does anyone know what this warning means?
I could not observe any issue in download performance and my target MCU is really the right one which I selected when creating the project.
best regards
Guenter
----------------------------------------------------
Connection from "127.0.0.1" via 127.0.0.1
Copyright 2012 P&E Microcomputer Systems,Inc.
Command Line :C:\Freescale\KDS_3.0.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_2.0.8.201504092111\win32\pegdbserver_console -device=Freescale_KVx_KV46F256M15 -startserver -singlesession -serverport=7224 -interface=OPENSDA -speed=5000 -port=USB1 -conf
CMD>RE
Initializing.
Warning 17927. Target MCU mismatch. Download performance limited. See http://www.pemicro.com/opensda/pe_tools.cfm for information on debugging external processors.
Target has been RESET and is active.
CMD>CM C:\Freescale\KDS_3.0.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_2.0.8.201504092111\win32\gdi\P&E\supportFiles_ARM\Freescale\KVx\freescale_kv46f256m15_1x32x64k_pflash.arp
Initializing.
Warning 17927. Target MCU mismatch. Download performance limited. See http://www.pemicro.com/opensda/pe_tools.cfm for information on debugging external processors.
Initialized.
....
...
已解决! 转到解答。
Hi Guenter,
using the P&E OpenSDA, you cannot debug another processor on another board. The K20 device on your board is tight to the CPU ID on the board.
If you want to use the the OpenSDA circuit to debug a non-resident CPU, you need to use a different firmware.
Erich
PS: posts on that subject:
Debug External Processors with USBDM and Freedom Board | MCU on Eclipse
Hi Guenter,
using the P&E OpenSDA, you cannot debug another processor on another board. The K20 device on your board is tight to the CPU ID on the board.
If you want to use the the OpenSDA circuit to debug a non-resident CPU, you need to use a different firmware.
Erich
PS: posts on that subject:
Debug External Processors with USBDM and Freedom Board | MCU on Eclipse