I have a KDS project with 5 different build configurations. Each build configuration defines unique symbols based on final project type that are referenced throughout the code to include or exclude source code. When I set any build configuration as active and build the project KDS recognizes the appropriate symbols and works like a champ.
The problem is that when I am making changes to the code ALL of the source code is grayed out because the none of the symbols are set in code. When I now right-click on a variable or function and try to "Open Declaration" it no longer works.
Has anybody else run into this situation or know how to correct it?
I could define the appropriate symbols for each build configuration in the code as I was doing before but the reason I changed it in the first place was so that I would not screw up and forget to change the #define's to the correct settings before building.
I tried defining ALL of the symbol in the source but that made things even worse when I went to do a build. (MANY Errors due to all code being included!)
Thanks,
John Baker
Solved! Go to Solution.
Hello,
if you have that 'grayed out' code problem, I think you see an old Eclipse Indexer problem: see Fixing the Eclipse Index | MCU on Eclipse for the explanation and solution for it.
I hope this helps,
Erich
Hi John,
Once you have built/compiled the target, right click on the project folder the surf to Index->Rebuild to have the index registry rebuilt. I think that will work for you.
Yell if it doesn't.
Regards,
David
Hello,
if you have that 'grayed out' code problem, I think you see an old Eclipse Indexer problem: see Fixing the Eclipse Index | MCU on Eclipse for the explanation and solution for it.
I hope this helps,
Erich