Installed KSDK in KDS but SDK New Project option still grayed out?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installed KSDK in KDS but SDK New Project option still grayed out?

ソリューションへジャンプ
779件の閲覧回数
davidrea
Contributor II

Hello All-

 

New to KDS and the Kinetis ecosystem but very experienced with Cortex controllers and Eclipse-based IDEs...

 

I've just installed KDS on both Windows 7 and Ubuntu 14.04, followed by the KSDK using the Eclipse "Install New Software..." mechanism on both OSs. In both cases, when creating a new KDS Project, the Kinetis SDK option remains grayed out.

 

I followed the instructions in the KDS release notes, including restarting Eclipse (and, just to be sure, both machines) - is there anything else that needs to be done?

 

Thanks,
Dave

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
519件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hi,

the SDK supports only few processors. Which one did you try?

I expect you:

1) installed KDS

2) installed KSDK

3) installed the eclipse update from KSDK folder (KSDK_1.0.0\tools\eclipse_update\SDK_1.0.0-GA_Update_for_Eclipse.zip)

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
520件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hi,

the SDK supports only few processors. Which one did you try?

I expect you:

1) installed KDS

2) installed KSDK

3) installed the eclipse update from KSDK folder (KSDK_1.0.0\tools\eclipse_update\SDK_1.0.0-GA_Update_for_Eclipse.zip)

0 件の賞賛
返信
519件の閲覧回数
davidrea
Contributor II

Hello Libor - Yes, I followed the steps you outlined. I was trying with the LK25Z64xxx4 processor, but I see now that only K2x, K6x and KV3x controllers are supported.

Thank you,

Dave

0 件の賞賛
返信