I´m using KDS 3.0.0 and a S9KEAZ128AVLH MCU. I found the following methods that supposedly do this:
For the AsynchroSerial component: SetBaudRateMode
For I2C_LDD and CAN_LDD: SetClockConfiguration
The problem is there is no way to enable this methods. For the AsynchroSerial , for exemple, it says that I should choose a specific value from the Timing dialog box, but I already did that and the problem remains.
Can you help me on that?
Hi Marico,
it seems these two components does not support runtime pin re-connection. There is method "ConnectPin" provided in both components, but cannot be turned on.
The last option is to generate code for the component, copy generated code to different location and disable component in the project. This solution is not ideal, but may help in your case.
Regards
Marek
Hello Marcio,
When you setting the Baud rate type to "list of values", the method "AS1_SetBaudRateMode" will available :
Hope it helps!
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi, I did that but the method "AS1_SetBaudRateMode" still keeps unavailable. What else did you do?
and what about the others serials communications, like CAN_LDD and I2C_LDD? how can I make the SetClockConfiguration Method available?
Hi Alice, yes, it´s available and I sent the reply before I check this, sorry.
About CAN_LDD and I2C_LDD there is no way to change it´s clock in running time?
And going further: it is either possible to switch a pin configuration using processor expert? Like to inicialize as a GPIO and then set it as an ADC input in running time?
Hi Mario,
LDD components support dynamic pin configuration, but it is little bit tricky to configure it. It is intended for advanced users.
Here is example for CAN_LDD component:
Hope that helps.
Regards
Marek
Hi Marek,
I choosed PTA0 for ADC_LDD component (ADC0_SE0) and Init_KBI (KBI0). It worked for the ADC, but for the Init_KBI component it seems to be unavailable the "Ignore Constraints and Non-Critical Errors". I have attached the print screens,
please take a look:
Hi Marcio,
it seems dynamic pin configuration is supported for LDD components only.
Init method of the KBI component does not contain initialization of the pin(s), this initialization is shared in after-reset code, see void Common_Init(void)
Init_KBI.c module is static, it is not generated, but copied into project if not there. You can modify this module manually (add pin routing) and your changes should be preserved.
Marek
Hi Marek,
Ok, thanks.
I have one last issue: i tryed to share I2C_LDD with SPIMaster_LDD, followed the steps you mentioned but still having the conflicts error. I have attached some print screens for you to check the problem.
Regards,
Marcio.