Does KDS 3.1 or 3.2 run on Windows 10?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does KDS 3.1 or 3.2 run on Windows 10?

625件の閲覧回数
thomasedel
Contributor III

Does Kinetis Design Studio (KDS) 3.1 or 3.2 run on Windows 10?  If not directly, are there any workarounds that help with compatibility?  Has anyone had success running it on Windows 10?  Any comments would be appreciated.

ラベル(1)
0 件の賞賛
2 返答(返信)

346件の閲覧回数
shauldorf
Contributor V

I’m using KDS 3.1 on Windows 10. Six month ago (September 2015) there was a problem with PEMicro driver.

The problem has been solved (October 2015) with driver patch for windows 10.

I think that today it is included in PEMicro release.

Shaul

0 件の賞賛

346件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I have seen KDS 3.0.0 and KDS 3.2.0 working on a Windows 10 machine (myself having Windows 7).

I recommend 3.2.0, as it comes with the latest Windows drivers for P&E and Segger.

Erich