Disable Blue LED pin on FRDM-KL25 that's already used for SPI comms

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Disable Blue LED pin on FRDM-KL25 that's already used for SPI comms

跳至解决方案
1,459 次查看
fireflies_at_night
Contributor II

Hello,

I have a project on the FRDM-KL25 board that uses SPI0 communication on the Port D pins (see image below). 

fireflies_at_night_0-1694539305828.png


However, I see that I inadvertently end up powering the board's Blue LED pin on PTD1 when I configure for SCLK.
Long shot but is there any way I can disable this blue LED and also use this pin only for my SPI CLK? 
It can be pretty annoying at night because the light is SUPER bright! Any thoughts? 

Thanks in advance!

标记 (4)
0 项奖励
回复
1 解答
1,445 次查看
ErichStyger
Specialist I

I see two options: a) cut the trace of PTD1 to the LED or b) re

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,416 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @fireflies_at_night 

I agree with Erich's suggestion, cut it.

 

BR

Alice

0 项奖励
回复
1,446 次查看
ErichStyger
Specialist I

I see two options: a) cut the trace of PTD1 to the LED or b) re

0 项奖励
回复
1,348 次查看
fireflies_at_night
Contributor II
Brutal. Looks like that's the only way.
Thanks Erich!
0 项奖励
回复