Hello,
I have a project on the FRDM-KL25 board that uses SPI0 communication on the Port D pins (see image below).
However, I see that I inadvertently end up powering the board's Blue LED pin on PTD1 when I configure for SCLK.
Long shot but is there any way I can disable this blue LED and also use this pin only for my SPI CLK?
It can be pretty annoying at night because the light is SUPER bright! Any thoughts?
Thanks in advance!
解決済! 解決策の投稿を見る。
I see two options: a) cut the trace of PTD1 to the LED or b) re