Disable Blue LED pin on FRDM-KL25 that's already used for SPI comms

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Disable Blue LED pin on FRDM-KL25 that's already used for SPI comms

ソリューションへジャンプ
1,622件の閲覧回数
fireflies_at_night
Contributor II

Hello,

I have a project on the FRDM-KL25 board that uses SPI0 communication on the Port D pins (see image below). 

fireflies_at_night_0-1694539305828.png


However, I see that I inadvertently end up powering the board's Blue LED pin on PTD1 when I configure for SCLK.
Long shot but is there any way I can disable this blue LED and also use this pin only for my SPI CLK? 
It can be pretty annoying at night because the light is SUPER bright! Any thoughts? 

Thanks in advance!

タグ(4)
0 件の賞賛
返信
1 解決策
1,608件の閲覧回数
ErichStyger
Specialist I

I see two options: a) cut the trace of PTD1 to the LED or b) re

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,579件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @fireflies_at_night 

I agree with Erich's suggestion, cut it.

 

BR

Alice

0 件の賞賛
返信
1,609件の閲覧回数
ErichStyger
Specialist I

I see two options: a) cut the trace of PTD1 to the LED or b) re

0 件の賞賛
返信
1,511件の閲覧回数
fireflies_at_night
Contributor II
Brutal. Looks like that's the only way.
Thanks Erich!
0 件の賞賛
返信