Difference between the "Cross ARM C++ Compiler" and the "GNU ARM C++ Compiler"?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between the "Cross ARM C++ Compiler" and the "GNU ARM C++ Compiler"?

1,084件の閲覧回数
tharonhall
Contributor IV

It was suggested to me that the "Cross ARM C++ Compiler" is unique to KDS, and I should ask my question here:

 

Original Question:

 

What is the difference between the "Cross ARM C++ Compiler" and the "GNU ARM C++ Compiler"?

 

Is it a fork of the GNU? Does it support the same commands and pragmas as GNU?

 

I've had ZERO luck Googling this.

 

--------------------

Follow up Post:

 

I can note that since I posted this, I did see a comment somewhere that the Cross Compiler is derived from the GNU Compiler, but no explanation was given as to what the differences are.

 

ラベル(1)
タグ(6)
0 件の賞賛
0 返答(返信)